Motor Control Applications
Closed-loop motor control: An Introduction to Rotary Resolvers and Encoders
by Texas Instruments
Introduction
Is your motor spinning at the intended rate? Closed-loop
motor control systems continue to answer this question,
as there tends to be a closed-loop system implemented
wherever a motor spins. Whether the end system is an
automobile (assisted parallel parking with computer controlled
steering), a satellite (positions satellite to lock on
to a specific signal), or factory floor machinery (a pickand-
place machine), the position feedback sensor is an
intrinsic element in the total motor-control system. There
are many types of motor control, but this article discusses
two that implement an analog signal chain around the
position sensor: the resolver and the encoder.
Resolver
Before discussing the signal-chain solution for a resolver,
consider its basic operation in Figure 1. The resolver (in
this case, a transmitter unit), is made up of three distinct
coil windings: the reference, the sine (SIN), and the cosine
(COS). The reference winding is the primary winding that,
through a transformer known as the rotary transformer, is
excited by an AC voltage applied to the primary side of
the transformer. Since the rotary transformer then passes
the voltage off to the secondary side of the transformer,
no brushes or rings are needed. This increases the overall
reliability and robustness of the resolver.

The reference winding is mounted on the motor shaft.
As the motor spins, the voltage output from the SIN and
COS windings change according to the shaft position. The
SIN and COS windings are mounted 90® from each other
in relation to the shaft. As the reference winding spins, the
angle of difference between the reference and SIN/COS
windings change, represented as the theta rotation angle
or θ in Figure 1. The voltages induced upon the SIN and
COS windings are equivalent to the reference voltage multiplied
by the SIN winding and COS winding of angle theta.
The induced output voltage waveforms are shown in
Figure 2. They show the normalized voltage-output signals
from the SIN and COS windings, divided by the reference
voltage. Traditional reference voltages are anywhere in the
1- to 26-V range, and the output frequency range is
800 Hz to 5 kHz.1
It is now possible to determine the requirements for the
appropriate signal-chain devices. The signal chain needs to
be bipolar because to the signal swings below ground
(Figure 2). It must simultaneously sample two channels,
convert up to 5-kHz signals, and supply AC voltage to the
resolver for the reference winding. The optimum solution
is to implement two delta-sigma modulators, one for each
channel. The delta-sigma modulators sample at very high
frequencies (in the 10- to 20-MHz range), so the deltasigma
modulated outputs are averaged out and filtered to
achieve an acceptable resolution.

For the reference voltage or AC-excitation source, a
pulse-width modulation (PWM) signal applied directly to
the resolver is preferred. TI has a recommended solution
for this kind of implementation. A data converter such as
the ADS1205 or ADS1209 is preferred for the delta-sigma
modulator because both are designed for direct interface
to the resolver's SIN and COS windings. The data converter
also interfaces to a four-channel sinc filter/integrator
with a PWM signal generator output for the reference
winding, for example the AMC1210. Finally, a digital signal
processor (DSP) or real-time controller is needed to handle
all the various signals in addition to the motor control
system. One such option is the C28x-based C2000™
Piccolo™ F2806x microcontroller from TI. Figure 3 illustrates
a typical signal-chain solution.
Conclusively, a resolver is a very robust position sensor
for a control system that offers high accuracy possibilities
and long operating life. A disadvantage of the resolver is
its maximum rotational speed. Because resolver signal frequencies
tend to be less than 5 kHz, motor speeds need to
be less than 5,000 revolutions per minute.
Encoder
As with the resolver scenario, before going into the signalchain
implementation, is important to understand the
physical and signal-output characteristics of encoders.
Typically there are two types of encoders: linear and
rotary. Linear encoders are used for items moving only in
a single dimension or direction, and convert the linear
position into an electronic signal. These often are used in
conjunction with actuators. Rotary encoders are used for
items moving around an axis, and convert the rotary positions
or angles into electronic signals. Since rotary encoders
are used with motors (as motors rotate along an axis)
linear encoders are not covered in this article.
To understand the principle behind a rotary encoder,
first consider a basic optical rotary encoder. An optical
encoder has a disk with specific patterns mounted to the
motor shaft. The patterns on the disk either blocks light or
allows it to pass through . Thus, a light-emitting transmitter
is used along with a photocel receiver. The receiver
signal output can be correlated to the motor's rotary
position.

There are three common types of rotary encoders: absolute
position value, incremental TTL signal, and incremental
sinusoidal signal. For absolute position value rotary
encoders, the pattern on the disk is broken up into a very
specific pattern based on its location. For example, if the
absolute position encoder has a 3-bit digital output, it
would have eight different patterns, evenly spaced (Figure
4). Since this is on a disk and is evenly spaced out, the
spacing between each pattern is 360°/8 = 45°. Now the
position of the rotary motor is known to be within 45° for
a 3-bit absolute position value rotary encoder.
The output of the absolute position value rotary encoder
is already optimized for digital interfaces, so an analog
signal chain is not required.
For the incremental TTL rotary encoder, the pattern on
the disk outputs a digital high or low, which is a TTL signal.
As shown in Figure 5, the TTL-output disk pattern is
relatively simple compared to the absolute position value
rotary encoder, because it needs to represent only one
digital high or digital low. In addition to the TTL signal
there also is a reference mark which is essential in determining
the motor's current rotary position. The reference mark can be thought of as angle 0°. Thus, simply counting
the digital pulses can determine the exact rotary position
of the motor.
Figure 5 illustrates multiple periods in one revolution of
the motor shaft. Encoder manufacturers offer incremental
TTL rotary encoders (and incremental sinusoidal rotary
encoders) with 50 to 5,000 periods per revolution. As with
absolute position value rotary encoders, the output is
already in a digital format, so no analog signal
chain is required.
For the incremental sinusoidal rotary encoder, the output
and disk pattern is quite similar to the TTL-signal
encoder. Instead of a digital output, the output is what the
name implies: a sine wave output. Actually, it has both
sine and cosine outputs along with the reference mark
signal as shown in Figure 6. These outputs are all analog,
so an analog signal-chain solution is required.
Similar to the incremental TTL output, there are multiple
signal periods in one revolution. For example, if the
encoder with 4,096 periods in one revolution is selected
and attached to a motor spinning at 6,000 revolutions per
minute, the resulting sine and cosine signal frequencies
can be calculated.
A signal-chain solution needs to have a bandwidth of at
least 410 kHz for this example. Since this is a closed-loop
control system, latency must be kept to a minimum or
completely eliminated. Traditionally, the encoder output
is 1 VP-P, and the sine and cosine output signals are
differential.
The typical requirements for the analog signal-chain
solution are:
- Two simultaneously-sampling analog-to-digital converters
(ADCs): One for sine and one for cosine outputs.
- No system latency: More than 400 kHz of bandwidth are
needed, thus an ADC must handle 800 kSPS per channel
minimum.
- 1-VP-P differential input with a full-scale range of around
1 V to optimize the ADC's full-scale range, or amplification
of the input signal to the ADC's full-scale range.
- A comparator for the reference-mark signal.
The optimum solution from TI is the ADS7854 family of
successive-approximation register (SAR) ADCs (Figure 7).
With two simultaneously-sampling channels, an internal
reference and 1-MSPS per channel output data rate, this
SAR-ADC meets the specified requirements. It can be
used with a comparator and a fully-differential amplifier to
drive the ADC.
Because the ADS7854 is a 14-bit ADC, and if the sinusoidal
incremental rotary encoder has 4,096 periods in one
revolution, the total number of measuring steps can be
calculated.
This gives the designer 26-bits of resolution when implementing
this approach, or accuracy of the rotary position
to within 5.36 × 10-6 degrees.
Conclusion
There are two common implementations of rotation/position
sensors in a motor-control feedback path: a resolver
and an encoder. The feedback path and output signal
characteristics of several control systems were evaluated
from the analog signal-chain perspective for either a
resolver or encoder to ensure signal integrity and optimum
performance.
References
- Advanced Micro Controls, Inc. (AMCI), "What is a
Resolver?" Available: www.amci.com/tutorials/tutorialswhat-
is-resolver.asp
- Texas Instruments. "Dual Channel Data Acquisition
System for Optical Encoders, 12 Bit, 1MSPS," TI
Prevision Verified Design. (06 June 2013). Available:
www.ti.com/2q14-tipd117
- Delta Computer Systems, "Resolver Fundamentals"
Available: www.deltamotion.com/support/
- HEIDENHAIN Brochure, "Rotary Encoders," November
2013, p. 13. Available: www.heidenhain.com/
Article written by Dwight Byrd, Precision Data Converters, Texas Instruments