Mouser Electronics Now Stocking STMicroelectronics' STKNX Miniature KNX Transceiver for Building Automation
July 24, 2018 - Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking the STKNX miniature KNX transceiver from STMicroelectronics (ST). Certified for the KNX standard for smart building automation applications, the STKNX is the smallest transceiver on the market certified for KNX TP1-256 twisted-pair connections, with power circuitry on-chip in a compact form factor of just 4mm × 4mm.
KNX is a standardized network communications protocol for building automation applications, widely adopted by several multinational and international standards. KNX twisted-pair wiring is inherited from the BatiBUS and EIB Instabus home automation standards. The ST STKNX miniature KNX transceiver, available from Mouser Electronics, allows developers to bring building automation products to market quickly, offering a complete network-node solution and KNX software stack compatible with any ST STM32 microcontroller.
The space-saving, highly integrated solution features two integrated voltage regulators — one with a selectable 150 mA high-efficiency DC/DC switching converter and one 3.3 V / 5 V 20 mA linear regulator — for external application use. An integrated KNX bus power extractor supports the power requirements of the transceiver as well as those of external devices. The STKNX transceiver ensures safe coupling to the bus and provides a monitoring warning for loss of bus power.
The transceiver is supported by the ST EVALKITSTKNX evaluation and development kit, available to order from Mouser. The kit contains everything needed to build a KNX node, including an STM32F103RBT6 microcontroller, Arduino-compatible headers for custom function expansion, and a sample LED-dimming application.
The STKNX transceiver combines energy efficiency, security and an enhanced user experience to facilitate the rapid development of smart home and smart building applications, including smart lighting, appliances, alarms, and HVAC controllers.
To learn more about the STKNX transceiver, visit www.mouser.com/stm-stknk-transceiver. For more information on the EVALKITSTKNX evaluation and development kit, go to www.mouser.com/stm-evalkitstknx-kit.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 700 manufacturers. Mouser offers 23 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in more than 220 countries/territories from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com